Want more insights on fluid system solutions? Our blog is packed with expert advice, industry trends, and practical tips to help you optimize performance. Explore more articles on our blog page!
Learn how to use the Swagelok M200 Orbital Welder for precise, high-quality welds. This guide covers key steps for setting up and executing orbital welding, ideal for industries like oil and gas, medical devices, and semiconductor manufacturing. Discover why this orbital welding machine is a game-changing tool for precision and reliability.
The Swagelok M200 is a portable orbital welding system designed to automate GTAW (Gas Tungsten Arc Welding) on tubing and pipe. Using a 360° rotating welding arc, this orbital welding system delivers consistent, high-quality welds without the need for manual intervention. It's ideal for industries like aerospace, semiconductor, and chemical processing that require reliable and efficient orbital tube welding.
Before starting the orbital welding process, gather and review all necessary documentation, such as heat numbers, drawings, and build instructions, to ensure everything is accurate for quality assurance.
After confirming the documentation, select the appropriate weld head based on the project’s requirements. Set up the welding system, ensuring the equipment is ready, including all power settings and safety checks, before proceeding with the welding process.
Position the first joint into the fixture block and clamp it securely in place. Carefully align the second joint in the same fixture and clamp it down as well to ensure both parts are aligned for the orbital weld. Proper alignment is crucial in orbital welding to ensure that the weld head moves smoothly along the joint, producing a precise, high-quality weld.
Place the restrictor on the outlet side of the tubing, then connect the purge gas, typically argon, to the inlet side and turn it on to prepare the weld area. After that, place the M200 weld head onto the fixture block, ground it, and latch it securely in position. This setup helps maintain a clean environment inside the tube, preventing oxidation during the welding process.
Once everything is set up, the welder will initiate a pre-purge cycle for 10 seconds to clean the internal tubing. A pulse purge follows for another 10 seconds to ensure no contaminants are present. The orbital welding process is then automatically executed by the M200, producing a clean, consistent weld.
After the weld is complete, remove the purge system and unclamp the assembly from the fixture. Use a brush to clean the welded area and remove any residue. The assembly is then inspected, subjected to helium leak testing, and passed on for final inspection, cleaning, and packaging before being sent for use or shipment.





By utilizing orbital welding techniques with the Swagelok M200 orbital welding machine, industries such as oil and gas, medical device manufacturing, and semiconductor production are able to achieve high-precision, repeatable welds that meet the highest standards of quality and reliability. This game-changing technology ensures that every weld is performed with the utmost consistency, making it an invaluable tool in the most demanding environments.
Want to learn more? Contact Us Today